RJ45 cable for connecting PSTB softstarter to the PSTEK External Keypad.
Good morning
I'm hoping you can help me. I have a PSTB1050-600-70 Softstarter and need to connect it to my PSTEK External Keypad but I don't have the interconnecting RJ45 coms cable. I can’t find a part number for the cable nor any information relating to it.
If you were able to find the wiring diagram I could make one myself and that would be great.
PSTB1050-600-70 - Part number 1SFA894020R7000
PSTEK - Part number 1SFA899003R1000
Thank you.
Answers
This question has not yet been answered.
by Amal Rank: 84 on 7/3/2020 5:09:53 AM | Like (0) | Report
Sir
I have seen your many questions about the same and I think it is getting disappearing from the forum because of duplication
I am no one to solve your issue but as per my experience in AKS it is always better to contact local abb support if you are not getting an answer from AKS and the issue is in priority of time
by john Rank: 2275 on 7/3/2020 6:59:23 AM | Like (0) | Report
I started with ABB support and sales and they couldn't help as there is no part number for just the cable.
Thanks for taking the time to reply, I was hoping that at least one of the AKS experts would have contacted me by now!
Add new comment