ABB ACS 560
Hi Experts,
I'm unable to run my ABB ACS 560 drive in the local mode it shows the direction lock symbol when I put into local mode even though there is no active fault or alarm in a drive, can anybody tell me which parameters should I check? I've checked the local mode activation parameters that are set ok to "0"
Please suggest.
I'm unable to run my ABB ACS 560 drive in the local mode it shows the direction lock symbol when I put into local mode even though there is no active fault or alarm in a drive, can anybody tell me which parameters should I check? I've checked the local mode activation parameters that are set ok to "0"
Please suggest.
Answers
Hi
Try to check how the parameters of group 20 are set, in particular on 20.12, 20.19 and 20.22
BR
Flavio
Try to check how the parameters of group 20 are set, in particular on 20.12, 20.19 and 20.22
BR
Flavio
Add new comment