ACS880 balancing?
Hi!
Im want to achieve a bumpless transfer between torque and speed-control when using the built-in controllers in ACS880. There is balancing functions for this purpose, see p.25.09 and p.25.10. According to the function diagrams the p25.09 is used for switching between speed controller output and balancing value.
But what happens when I switch it back, is the value in p.25.10 copied to p.25.57 controller output, otherwise a bumpless transfer is not acchieved anyway?
Best regards Magnus Bergsten
Im want to achieve a bumpless transfer between torque and speed-control when using the built-in controllers in ACS880. There is balancing functions for this purpose, see p.25.09 and p.25.10. According to the function diagrams the p25.09 is used for switching between speed controller output and balancing value.
But what happens when I switch it back, is the value in p.25.10 copied to p.25.57 controller output, otherwise a bumpless transfer is not acchieved anyway?
Best regards Magnus Bergsten
Answers
This question has not yet been answered.
Add new comment