Softstarter PSE show Error SF34 on display.
Hi all, If my new PSE softstarter show Error SF34,
By-pass relay does not open or thyristor short
circuit
How should I solve it? as it keep show up on display after reset. Any possiblilty like connection problem or motor can lead to this problem?
Thanks
Answers
Hi
first, also to help us understand what it is, always write the motor type and power, the precise model of the soft starter and if the error signal occurred immediately, as soon as you connected it or after some time of operation and following what circumstances.
Have you tested the cable and the motor?
Have you tried to connect another motor to the soft starter?
If you provide more information, maybe we can help you better
BR
Flavio
first, also to help us understand what it is, always write the motor type and power, the precise model of the soft starter and if the error signal occurred immediately, as soon as you connected it or after some time of operation and following what circumstances.
Have you tested the cable and the motor?
Have you tried to connect another motor to the soft starter?
If you provide more information, maybe we can help you better
BR
Flavio
Add new comment