800xA 6.0.3-0 is giving issue while adding nodes to it.
We have installed ABB 800xA Base 6.0.3-0 in Windows 10 LTSB Machine, made the system as primary Aspect and connectivity system.
Then install the software in other machine and connected this in network. The system is configured in Work group. following are the issues coming
1. The node is not getting detected in main machine(Aspect and connectivity System).
2. RNRP showing system is up. but host files are not getting updated.
3. After typing the name in Primary Aspect and connectivity machine we were able to add. and node became healthy. but when we reboot the system the Afw Service Connection Status is coming disabled in client machine.
4. we are installing the the software directly through media we got.
Then install the software in other machine and connected this in network. The system is configured in Work group. following are the issues coming
1. The node is not getting detected in main machine(Aspect and connectivity System).
2. RNRP showing system is up. but host files are not getting updated.
3. After typing the name in Primary Aspect and connectivity machine we were able to add. and node became healthy. but when we reboot the system the Afw Service Connection Status is coming disabled in client machine.
4. we are installing the the software directly through media we got.
Voted best answer
The check box Register this connection's addresses in DNS must be checked for the Client Server Network
![]()
Answers
Hello,
there are many reasons.
try by conencting directly between each other
there are many reasons.
- check the host based firewalls status -try by disable them
- check Network connections as a basic to check both are having same series of IP and able to ping each other.
- Check agents are installed--see the logs for more clue
- check network switch settings to meet the RNRP requirements
try by conencting directly between each other
Add new comment