3 PLC and SCADA PC
Hi,
Sorry if I asked this question on the wrong forum
I have 3 PLC which are placed in different sites and PC where the SCADA and OPC (Kepware) is installed
All PLC are having Ethernet port
I'm using Modbus TCP/IP to achieve data collection. As to get these data my 3 PLC and my PC should be in the same IP network?
Can anyone have a solution for this? How can I make the 4 in the same network?
Regards
Amal
Sorry if I asked this question on the wrong forum
I have 3 PLC which are placed in different sites and PC where the SCADA and OPC (Kepware) is installed
All PLC are having Ethernet port
I'm using Modbus TCP/IP to achieve data collection. As to get these data my 3 PLC and my PC should be in the same IP network?
Can anyone have a solution for this? How can I make the 4 in the same network?
Regards
Amal
Answers
This question has not yet been answered.
Add new comment