Backup problem
I have started taking backup of control structure but while including dependencies it ask the memory limit as attached in pic.please tell how it will be better option for taking backups.
Voted best answer
To answer the question: "How I will split large exports in smaller archives?"
When not including dependencies, I will assume that you will be able to export the whole e.g. [Control Structure]Root into one export archive.
Otherwise you will simply have to split up the export of e.g. Control Structure into several export archives.
From the example screen dump of a Control Structure, I would suggest to export "Network 11A, MB300 Network" in one separate export archive and export "Network 11B, MB300 Network" in another separate export archive.
I hope the above might help you.
Best regards
Carsten
When not including dependencies, I will assume that you will be able to export the whole e.g. [Control Structure]Root into one export archive.
Otherwise you will simply have to split up the export of e.g. Control Structure into several export archives.
From the example screen dump of a Control Structure, I would suggest to export "Network 11A, MB300 Network" in one separate export archive and export "Network 11B, MB300 Network" in another separate export archive.

I hope the above might help you.
Best regards
Carsten
Answers
Hi
In case you want to include dependencies, it is recommended to split large exports into smaller archives.
My recommendation is not to include dependencies. I can't remember a situation when importing that dependencies would have been necessary / to prefer.
I hope that you will find it sufficient to export without dependencies.
Best regards
Carsten
Do you have a limit of the disk space?
Usually even a full system backup is not so big according to the disk space available these days.
My experience shows, that control structure backup with dependencies finishes fast and have an acceptable size.
Add new comment