NDC MATRIX NOT SHOWING NODE NAME
I HAVE UPGRADE THE COMPOSER 4.3 PROJECT IN S+ ENGINEERING 2.2, and then designed the Topology Design of the Project synchronized with OE and then went to NDC Matrix where i didn't see the node name and other Details.
Please brief what else i have to do, we have traditional Infi Net and Control Unit with NIS|NPM.
Please brief what else i have to do, we have traditional Infi Net and Control Unit with NIS|NPM.
Answers
If you select the S+ Operations server with HSI Server or Front end server profile in spo function, then this node gets listed in ndc matrix.
Rack based modules are not supported in Topology design. But nodes (computer with/without monitor) and network can be defined.
Rack based modules are not supported in Topology design. But nodes (computer with/without monitor) and network can be defined.
Source: System Topology user manual
Did you add plantarea in your toplogy design diagram? Try add a plantarea and include your device in the area.
Hi,
Maybe the Node Database is not filled up by the "Synchronized with OE" check if node database contains nodes definition, if not repeat the operations or remove and re insert the node and make "Synchronized with OE" again.
Maybe the Node Database is not filled up by the "Synchronized with OE" check if node database contains nodes definition, if not repeat the operations or remove and re insert the node and make "Synchronized with OE" again.
the attached snap as a reference for your information
@alesandaro n @ALL please note the attached image as reference
by itron Rank: 122 on 6/8/2020 12:46:02 AM | Like (0) | Report
Dear All I have also assigned the Plant Area in the Topology Design, but coundn't see the same in NDC Matrix
Add new comment