Three Screen Navigation issue due to Tabbed Navigation
I have to raise this one again , as we are not able to solve this issue
1) 3 screens are configured , tab navigation is provided in all 3 screens -> when click the tab navigation on 2nd and 3rd screen display open on the the first screen -> this is very much difficult for the operators as we are using EOW -X3
We are not facing any issue with Normal navigation -> its only with Tab navigation
2) Any object (Faceplate/Alarm) right click Context menu is opening on the 3rd screen right corner -> which make more difficult for operator to select alarm/trend aspect.
Can any one help to solve this issue
1) 3 screens are configured , tab navigation is provided in all 3 screens -> when click the tab navigation on 2nd and 3rd screen display open on the the first screen -> this is very much difficult for the operators as we are using EOW -X3
We are not facing any issue with Normal navigation -> its only with Tab navigation
2) Any object (Faceplate/Alarm) right click Context menu is opening on the 3rd screen right corner -> which make more difficult for operator to select alarm/trend aspect.
Can any one help to solve this issue
Answers
You can try to Import a multiscreen workplace.
Templates for Multiple Screens A set of pre-configured templates with Operator Workplaces using multiple screens are available in System 800xA. These are available as import files. These import files are found in the directory: Program Files\ABB Industrial IT\Operate IT\Process Portal A\importExamples\MultiScreen Workplaces.
Templates for Multiple Screens A set of pre-configured templates with Operator Workplaces using multiple screens are available in System 800xA. These are available as import files. These import files are found in the directory: Program Files\ABB Industrial IT\Operate IT\Process Portal A\importExamples\MultiScreen Workplaces.
Add new comment