CI873 communication error. Lost communication during normal activity
Hello,
In a project, we have an issue with one CI873 module. from time to time it losses communication and when we see the module log, we see the following message from all the slaves connected to it.
I 2020-05-13 14:32:06.315 (tEipRcvTsk)[DIGITALIODRV] MSG_REG_INPUT_ASSEM 2 I 2020-05-13 14:32:06.315 (tEipCnfgRcvTsk)[DIGITALIODRV] NM_CONN_CONFIG_FAILED_INVALID_NETWORK_PATH_2 :5.2. I 2020-05-13 14:32:06.318 (tEipRcvTsk)[DIGITALIODRV] MSG_CONN_DROPPED - CONNID 2 I 2020-05-13 14:32:06.323 (tEipSndTsk)[DIGITALIODRV] MSG_REG_OUTPUT_ASSEM 2
Please your advice
In a project, we have an issue with one CI873 module. from time to time it losses communication and when we see the module log, we see the following message from all the slaves connected to it.
I 2020-05-13 14:32:06.315 (tEipRcvTsk)[DIGITALIODRV] MSG_REG_INPUT_ASSEM 2 I 2020-05-13 14:32:06.315 (tEipCnfgRcvTsk)[DIGITALIODRV] NM_CONN_CONFIG_FAILED_INVALID_NETWORK_PATH_2 :5.2. I 2020-05-13 14:32:06.318 (tEipRcvTsk)[DIGITALIODRV] MSG_CONN_DROPPED - CONNID 2 I 2020-05-13 14:32:06.323 (tEipSndTsk)[DIGITALIODRV] MSG_REG_OUTPUT_ASSEM 2
Please your advice
Answers
This question has not yet been answered.
Add new comment