TA521
Greetings
What is the use of TA521
If anyone can share what is the use of it and where it uses?
What is the use of TA521
If anyone can share what is the use of it and where it uses?
Voted best answer
Hi
TA521 is a backup battery for the AC500 CPU series and is used when it is necessary to have a backup of the data - for example variables configured as retention - in the absence of PLC power supply
BR
Flavio
TA521 is a backup battery for the AC500 CPU series and is used when it is necessary to have a backup of the data - for example variables configured as retention - in the absence of PLC power supply
BR
Flavio
Add new comment