800xA System 6.0.3-3 with RU6 and TC2 installed. - How to remove ghost service providers?
Hello all,
We performed the upgrade from a system version 4.1 to version 6.0.3-3. During the SAT, we identified that some ghost service providers exist on the service structure, as you can see on the attached pictures.
I can not edit, view or remove these providers. If we run the command "Afwsct.exe -c ", then we can identify these providers as a failure of consistency the service structure.
Does anyone ever face this kind of problem before? Any idea of how to fix it?
Best Regards
Diego
We performed the upgrade from a system version 4.1 to version 6.0.3-3. During the SAT, we identified that some ghost service providers exist on the service structure, as you can see on the attached pictures.
I can not edit, view or remove these providers. If we run the command "Afwsct.exe -c ", then we can identify these providers as a failure of consistency the service structure.
Does anyone ever face this kind of problem before? Any idea of how to fix it?
Best Regards
Diego
Answers
If you can't remove them by clicking the Delete/Remove button in the Service Group aspect, nor by running afwsct with "-c" (correcting mode) it is time to file an official support case with your regional ABB support center.
Add new comment