Configure AC800M 6.1 Soft Controller with Controller IP
Is it possible to configure AC800M 6.1 Soft Controller with Controller IP address ?
Think about creating a windows 10 virtual machine with a controller IP address configured (ex: 172.16.80.151). 800xA 6.1 Soft controller installed on windows 10 machine. How to remove the MMSProcessVariable number from soft controller ? MMSProcessVariable configuratable from 2 to 45.
Is there any way to do that ? I want my soft controller IP address as "172.16.80.151" not as "172.16.80.151:2"
Any suggestions appreciable.
Think about creating a windows 10 virtual machine with a controller IP address configured (ex: 172.16.80.151). 800xA 6.1 Soft controller installed on windows 10 machine. How to remove the MMSProcessVariable number from soft controller ? MMSProcessVariable configuratable from 2 to 45.
Is there any way to do that ? I want my soft controller IP address as "172.16.80.151" not as "172.16.80.151:2"
Any suggestions appreciable.
Answers
This question has not yet been answered.
Add new comment