PROJECT DOWNLOAD PROBLEM IN CONTROL BUILDER WITH SOFT CONTROLLER
I HAVE TAKEN ACRONICS BACKUP OF AN ENGINEERING STATION PC.THEN I RUN IT ONTO MY PC THROUGH VMWARE WORKSTSTION.
PROBLEM IS WHEN I WANT TO DOWNLOAD THE PROJECT WITH CONTROL BUILDER VIA SOFT CONTROLLER TO VISUALIZE MY SCADA THEN IT SHOWS SOME ERROR."9159 "
MY CONTROL BUILDER VERSION IS 5.1.1
SOFT CONTROLLER VERSION IS V5.1
HOW CAN I DOWNLOAD MY PROJECT IN THE CONTROLLER BUILDER TO VISUALIZE THE SCADA.
COULD YOU PLEASE TELL ME THE PROCESSURE.
REGARDS
RISLU
Voted best answer
Hello,
can you share some snaps showing the error.
Sometimes mms starts works after you establish the temporary connection (connect your bridged network to any switch/other PC) and try download.
can you share some snaps showing the error.
Sometimes mms starts works after you establish the temporary connection (connect your bridged network to any switch/other PC) and try download.
Answers
Hi,
Refer the below link
BR
ATP
Refer the below link
BR
ATP
The Soft Controller will not start unless you have an active Ethernet Interface with a "Cable" plugged into it. The controller binds to the IP address set on the card. Since you have a VM, make sure the Port Address on the Virtual Machine's interface card is set correctly and that port is connected in the VMware settings.
Add new comment