E_AFW_SI_SEC_NOT_INITED(0x8abb1003) Security not initialized on node
Hi,
Im installing an upgrade of a 800xA system, the original version is a 5.1, and the new is a 6.0.3, because of some problems, once i already have the system ready, y have to format and reintall both Aspect servers, with the same configuration, but at the moment of adding all of the others servers, the config wizard send this message at first:

after i performed a 'System software User settings', this message change to the next one:

already check the firewall, and time sync, both aspect server, are already in the system, both all of the others nodes send the message of the last picture.
i have already check the topic that ask the same thing, but none of the answers solve the problem (this link). if anyone have any information about this, it would help a lot.
Regards.
Im installing an upgrade of a 800xA system, the original version is a 5.1, and the new is a 6.0.3, because of some problems, once i already have the system ready, y have to format and reintall both Aspect servers, with the same configuration, but at the moment of adding all of the others servers, the config wizard send this message at first:

after i performed a 'System software User settings', this message change to the next one:

already check the firewall, and time sync, both aspect server, are already in the system, both all of the others nodes send the message of the last picture.
i have already check the topic that ask the same thing, but none of the answers solve the problem (this link). if anyone have any information about this, it would help a lot.
Regards.
Answers
Are you using the procedures outlined in the 6.0.3 Installation and Upgrade Manual?
The classic Configuration Wizard is hardly ever used to install 6.0 and onwards.
The classic Configuration Wizard is hardly ever used to install 6.0 and onwards.
by elemravi Rank: 33 on 4/21/2020 6:25:00 PM | Like (0) | Report
Just to clarify: I believe your system version is 6.0.3. Which tool are you using to add nodes? AFWConfigWizard or System configuration console?
by Rajeev1502 Rank: 56 on 4/21/2020 11:26:02 PM | Like (0) | Report
have you performed replace node function from SCC.
Add new comment