Functional block in 800XA version 6.03
Is there any functional block for programming in fbd in 800XA version 6.03 for matching the output (4-20mA) from instrument exactly as displayed in pg2 graphics.Also this signal is taken in addition with another (4-20mA) output ssignal and display total value by using these signals with counters.so that whatever total value comes its 1st output should match the values of total o/p 1st signal output.This operation should perform in automode.
Answers
This kind of project specific solutions require user defined Function blocks.
If the same solution is expected in more than one project, you can standardise that module for reusing it.
Add new comment