800xA Ruler Value Format
Dear All,
In 800xA trend display, the rular value is shown as a true value without diecmal digits!
who can i change the format of the ruller?
thank you in advance.
Abdelrazzaq Hiasat.
In 800xA trend display, the rular value is shown as a true value without diecmal digits!
who can i change the format of the ruller?
thank you in advance.
Abdelrazzaq Hiasat.
Answers
This question has not yet been answered.
by Stefan Stromqvist
Can you add an image?
What is the source of the property you are trending?
You may have to use a Property Extension Info aspect unless the property has built-in presentation info.
Examples of properties with built in support for presentation attributes (no PEI required):
- "RealIO" of AC 800M
- MB300 AI of AC450
Examples of properties without built in support for presentation attributes (PEI is required):
- float of AC 800M
- General Property of 800xA Base
Add new comment