How can i export and import application configuration of one IED in PCM600.
I am using the PCM600 2.9 version. I want to export only the logic code written in one IED configuration. please help.
Answers
Hi.
Application Configuration export files are called MainApplication Templates in PCM600. In PCM600 2.9 you can export such a template when Application Configuration tool is open by selecting from the Main Menu > File > MainApplication Template > Export.
For more information, please see the PCM600 2.9 Operation Manual Chapter 3.3.13.
Application Configuration export files are called MainApplication Templates in PCM600. In PCM600 2.9 you can export such a template when Application Configuration tool is open by selecting from the Main Menu > File > MainApplication Template > Export.
For more information, please see the PCM600 2.9 Operation Manual Chapter 3.3.13.
Add new comment