Unable to open Safety PLC (SM560-S) program on Automation Builder V2.2.0
Hi guys,
I'm new to ABB platform, so this is probably a noob question.
I'm trying to open a copy of the code from a client which a safety and non-safety programs. I've managed to open the non-safety program without any issues using the trial version of Automation Builder 2.2.0 however struggling to open safety program (SM560-S) does not open.
Possible issues:
1. I believe the existing code is from version 1.1.0 - I've converting the code and opening on V1.1 but it didn't work. The Automation Builder immediately shutdown after a warning stating " The project contains objects that are not supported by the current installation: XXX_Safety_Application. Please install the appropriate packages.". I assume the device EDS is missing but I am not sure where to find/download them..
2. In version 2.2.0, there is option under Tools-> Device Repository -> Download missing device but when i select download - the download just fails. Is SM560-S not available for Automation Builder V2.2.0
Any help will be greatly appreciated. Thanks.
Regards,
Paras

Answers
IMHO the trial version can't open a Safety Project. Probably you need a specific licence to open this project. I suggest you to contact you nearest ABB dealer to have the correct support.
BR
Flavio
Add new comment