NO OPTION AVAILABLE FOR DELETING PROJECT FROM RECENT TAB
DEAR SIR WE USE FREELANCE 2019.THERE ARE 2 PROJECTS SHOW IN RECENT TAB. I WANT TO DELET ONE OF THEM BUT NO OPTION AVAILABLE AFTER RIGHT CLICK ON SELECTED PROJECT. PLESE PROVIDE SOLUTION.
You must use the delete option in the window section below. The project must be marked in the upper part of the window (outlined in blue) and then call the options menu in the lower window with the right mouse button
Add new comment