PCM 600 2.9
I have installed PCM 600 2.8 and PCM 600 2.9 along with hotfixes on VMWARE windows 7 Machine I run PCM 2.8 without any issue, but when I try to run PCM 2.9 I get the message:
Some of the binary files are not signed with a valid ABB certificate, this may indicate an attempt to manipulate PCM 600 installation and could result with unwanted behaviour.
I tried to reinstall PCM 2.9 again but it gives me the same message when I want to run it.
Some of the binary files are not signed with a valid ABB certificate, this may indicate an attempt to manipulate PCM 600 installation and could result with unwanted behaviour.
I tried to reinstall PCM 2.9 again but it gives me the same message when I want to run it.
Answers
Hi. Uninstall PCm600. Install SQL server applicable for PCM600 2.9version. Then you install PCM
Hi,
please start by running Windows Update on your system, it seems that root certificates are not up to date on the system.
If that doesn't help, please contact your local ABB.
--
Markku
please start by running Windows Update on your system, it seems that root certificates are not up to date on the system.
If that doesn't help, please contact your local ABB.
--
Markku
Add new comment