INSTALLATION OF ABB Excel Add-In ON A CLIENT WORK STATION BASED ON WIN 7 for 800xA system
i am ABB engineer working on 800xA project, We have installed ABB Excel Add-In on the A client Work stations that is connected to the PIMS over the Public network to collect history data, on Windows 7. Due to information security reasons all the client workstation on the network were upgraded to Windows 10. After the upgrade we could not install the ABB Excel add-in on client personal workstations.
Please advise about the following;
- It is possible to upgrade the Excel add-in only without updating the whole DCS system?
- Is there is other way to install the ABB Excel ADD-IN “Data Direct” on Windows 10, without upgrade?
Answers
Without making a formal statement, it is usually possible to run with a more recent version of DataDirect compared to what version you have of AdvaInform Display Services in the Information Manager, part of the 800xA System.
Add new comment