AC800F controller can not modify IP adress,why?
i switch run/stop to stop,there is not have modify IP adress menu,can not modify ip adress,why?
log:
PFail Initialize: ....... +--------------------------------------------------------------------+ | | | | A B B | 1st Stage >> Startup Operation Checkout << | | | 1st Stage version: F04.102.00, Aug 26 2016 | | | EPROM version : 10.30 | | | Buildindex : 9142 | | AC800F (PM803F) | (C) 1998...10 ABB Automation GmbH | | | | +--------------------------------------------------------------------+ Hardware initialized FPGA revision 02.64(0) EPLD revision 20 Diagnostic interface.....: OK Testing checksum EPROM...: OK Testing SRAM WORD access......: OK BURST access.....: OK address lines....: OK Testing EDC Unit.........: OK Enabling EDC Unit... Testing counter..........: OK *** Internal selftest completed, 1st Stage is activating Bootloader... *** ABB ** AC 800F/16 ** BootLoader V10.30 (C)2002 ABB Automation Products 19 Sep 2015 T.Guenther Testing network connection 1 ... Ok Testing network connection 2 ... Ok ------------------------------------------------------------------------------ CPU is i960HT [B0/B1] with 16 MByte RAM System will startup in AUTO mode First Network Interface [00:C0:C9:11:64:96] - TwistedPair - IP address: 172.16.1.1 - Subnet mask: 255.255.240.0 Second Network Interface [00:C0:C9:11:64:64] - TwistedPair as RedLink RTC-Time: 30.03.20, 10:39:30 local ------------------------------------------------------------------------------ <C>hange, set <T>ime, <S>ave or continue <B>ooting? c For each of the following questions hit <RET> to keep the value in braces or enter a new value: Enter startup mode: 1. Auto Startup 2. Force BootLoader execution Select: [1] Dump statistic on exit? [n] Log Downloads? [n] Enter baud rate of console port: [9600] 9600 Enter CPU delay (in seconds) before starting up: [2] 2 ------------------------------------------------------------------------------ CPU is i960HT [B0/B1] with 16 MByte RAM System will startup in AUTO mode First Network Interface [00:C0:C9:11:64:96] - TwistedPair - IP address: 172.16.1.1 - Subnet mask: 255.255.240.0 Second Network Interface [00:C0:C9:11:64:64] - TwistedPair as RedLink RTC-Time: 30.03.20, 10:39:48 local ------------------------------------------------------------------------------ <C>hange, set <T>ime, <S>ave or continue <B>ooting? s Parameters saved
log:
PFail Initialize: ....... +--------------------------------------------------------------------+ | | | | A B B | 1st Stage >> Startup Operation Checkout << | | | 1st Stage version: F04.102.00, Aug 26 2016 | | | EPROM version : 10.30 | | | Buildindex : 9142 | | AC800F (PM803F) | (C) 1998...10 ABB Automation GmbH | | | | +--------------------------------------------------------------------+ Hardware initialized FPGA revision 02.64(0) EPLD revision 20 Diagnostic interface.....: OK Testing checksum EPROM...: OK Testing SRAM WORD access......: OK BURST access.....: OK address lines....: OK Testing EDC Unit.........: OK Enabling EDC Unit... Testing counter..........: OK *** Internal selftest completed, 1st Stage is activating Bootloader... *** ABB ** AC 800F/16 ** BootLoader V10.30 (C)2002 ABB Automation Products 19 Sep 2015 T.Guenther Testing network connection 1 ... Ok Testing network connection 2 ... Ok ------------------------------------------------------------------------------ CPU is i960HT [B0/B1] with 16 MByte RAM System will startup in AUTO mode First Network Interface [00:C0:C9:11:64:96] - TwistedPair - IP address: 172.16.1.1 - Subnet mask: 255.255.240.0 Second Network Interface [00:C0:C9:11:64:64] - TwistedPair as RedLink RTC-Time: 30.03.20, 10:39:30 local ------------------------------------------------------------------------------ <C>hange, set <T>ime, <S>ave or continue <B>ooting? c For each of the following questions hit <RET> to keep the value in braces or enter a new value: Enter startup mode: 1. Auto Startup 2. Force BootLoader execution Select: [1] Dump statistic on exit? [n] Log Downloads? [n] Enter baud rate of console port: [9600] 9600 Enter CPU delay (in seconds) before starting up: [2] 2 ------------------------------------------------------------------------------ CPU is i960HT [B0/B1] with 16 MByte RAM System will startup in AUTO mode First Network Interface [00:C0:C9:11:64:96] - TwistedPair - IP address: 172.16.1.1 - Subnet mask: 255.255.240.0 Second Network Interface [00:C0:C9:11:64:64] - TwistedPair as RedLink RTC-Time: 30.03.20, 10:39:48 local ------------------------------------------------------------------------------ <C>hange, set <T>ime, <S>ave or continue <B>ooting? s Parameters saved
Answers
Hello,
I see your current IP address is 172.16.1.1/255.255.240.0,
If new IP address you are going to set in 172.16.1.x, x = 1 - 14 and subnet mask is 255.255.240.0 i.e standard IP setting, then you can do so from rotary switch on E1 ethernet card.
If you want to set any other IP address e.g.192.168.0/255.255.255.0 i.e non-standard IP setting , then put rotary switch on E1 ethernet card to 0.
Then try what you are trying to do...
Also make use of AC800F installation and mounting manual.
And still no success, get connect to your local or regional L3 Tech. support center.
Hope that helps....
I see your current IP address is 172.16.1.1/255.255.240.0,
If new IP address you are going to set in 172.16.1.x, x = 1 - 14 and subnet mask is 255.255.240.0 i.e standard IP setting, then you can do so from rotary switch on E1 ethernet card.
If you want to set any other IP address e.g.192.168.0/255.255.255.0 i.e non-standard IP setting , then put rotary switch on E1 ethernet card to 0.
Then try what you are trying to do...
Also make use of AC800F installation and mounting manual.
And still no success, get connect to your local or regional L3 Tech. support center.
Hope that helps....
Add new comment