ACS 800 drive tripping with BR Wiring fault
DRIVE,ACS800-04-0210-3+D150 in Long travel of Crane.BR wiring fault is coming while operation.While in no load without DBR no fault is coming.So on doubt basis, change brake chopper card and IGBT (Chopper Ckt) but still problem is coming.
Answers
Hi
the description of the fault is unfortunately too concise, in addition to the checks you have made, a more in-depth analysis of the dxrive is required, which I advise you to have performed by the ABB service closest to you
BR
Flavio
the description of the fault is unfortunately too concise, in addition to the checks you have made, a more in-depth analysis of the dxrive is required, which I advise you to have performed by the ABB service closest to you
BR
Flavio
You should check Braking resistor(maybe it's damge) sửa chữa biến tần ABB
Add new comment