Communication variables between Applications in two controller (AC800M)
My objective to pass data/signal between controller of each Application program of different controller .
I had done set an communication variable ( Variable1 , direction:in , ip address:controller 2 for Application 1, Program1, Controller1, ) and ( Variable1 , direction:out, ip address:controller 2 for Application 2,Program1, Controller2).
I tried on test mode set value on Application 2 communication variable 1, but Variable 1 on Application 1 did not change according to follow Application 2.
Any help or explained much appreciated.
Voted best answer
Answers
Don't forget to put the controller in simulation mode and assign the system identity (via r-click context menu on controller) to the same IP address as the softcontroller + process id (ie 172.16.15.35:2)
Add new comment