install system instructions
Good morning
i have v6 compact HMI, when i do a backup on manteniance appear error
"system extension "system instructions" with id {xxxxxxxxxxxxx} is not installed in this node"
backup work well but i need clear this error
where i can install this extension?
system instructions
best regards
i have v6 compact HMI, when i do a backup on manteniance appear error
"system extension "system instructions" with id {xxxxxxxxxxxxx} is not installed in this node"
backup work well but i need clear this error
where i can install this extension?
system instructions
best regards
Voted best answer
I guess your system was an upgrade from version 5.0 (at some point)?
When upgrading to 5.0 SP2, this system extension, along with all Manuals in Product Type Structure, must be deleted from the system (at least for 800xA, it must be similar for Compact HMI).
Search for the AfwRemoveSystemInstructions.exe under the system bin folder path like C:\Program Files (x86)\ABB 800xA\Base\bin, executing this program should remove the reference to this extension from your system
When upgrading to 5.0 SP2, this system extension, along with all Manuals in Product Type Structure, must be deleted from the system (at least for 800xA, it must be similar for Compact HMI).
Search for the AfwRemoveSystemInstructions.exe under the system bin folder path like C:\Program Files (x86)\ABB 800xA\Base\bin, executing this program should remove the reference to this extension from your system
Add new comment