In the absence of the Mastergate product, what is the best way to exchange data between MB300 network controllers
Answers
Hello Bryce.
For the main Dataset functionallity, the recommendation is to replace the MasterGate 230/1 nodes with one AC800M controller and CI855 MB300 communication boards.
Please see my attached powerpoint for details.
The AC800M cannot be used for all features that the MG230/1 did offer, but it can be used for the most important Dataset functionallity.
For other functions such as Engineering from Plant Network and HMI on plant network (if used) there are other possibilities available, i.e. to use Remote desktop and
MultiSystemIntegration in 800xA.
For sales support, please contact the local ABB Sales organisation for your business area in your country.
I'm always available for them and is working globally with Advant Master Evolution.
E mail: jan-erik.rask@se.abb.com
Best Regards Jan-Erik Rask
Add new comment