Siemens S7-300 and ACS880
Hello everybody
I am using a siemens PLC S7-315 to control an acs880 with a FENA21 card ( profinet protocol). I am using PPO6
Could anybody tell me if it is possible to read the PZD parameters ( usually anolog values) with the siemens function SFC15 ( read cyclic data) ?
I have seen that ABB furnishes a library but it seems to be working only with S7-1500. Am I true ?
Thanks
Olivier
I am using a siemens PLC S7-315 to control an acs880 with a FENA21 card ( profinet protocol). I am using PPO6
Could anybody tell me if it is possible to read the PZD parameters ( usually anolog values) with the siemens function SFC15 ( read cyclic data) ?
I have seen that ABB furnishes a library but it seems to be working only with S7-1500. Am I true ?
Thanks
Olivier
Answers
Hello,
It is possible to read parameters from drive with SFC14, and write to drive with SFC15.
Add new comment