Installation problem, component FDSAspectSystem.DataCopied.1, error The specified module could not be found
System 800xA 5.1 Rev E FP4 RU4, We are getting many system events when we access any tag in 1no of Operating Station. This OS also have 3rd Party OPC Connection through Surrogate. When we open any faceplate, trend , graphic etc.it generates this type of events. This events also getting generated when we refresh Tags in Third Party OPC Client Application. Please suggest how to stop this events getting generated. Pics Attached for reference.
Answers
Likely, this client has not been installed with all system extensions that has been added to the system (which is a requirement).
The name hints Engineering Studio - Function Designer
By calling the System Extensions aspect in the Admin Structure from Plant Explorer running on this troublemaking client will tell what is missing, each row should have two crosses.

Also a DCT > Analyze > Analyze Software can also be used to spot a missing software component.
A component may also have become damaged - if all software seem installed, try repairing or reinstalling one or more components, e.g. Engineering Studio.
The name hints Engineering Studio - Function Designer
By calling the System Extensions aspect in the Admin Structure from Plant Explorer running on this troublemaking client will tell what is missing, each row should have two crosses.

Also a DCT > Analyze > Analyze Software can also be used to spot a missing software component.
A component may also have become damaged - if all software seem installed, try repairing or reinstalling one or more components, e.g. Engineering Studio.
Add new comment