How to change the reference speed of ACS800
Hi,
How to change the reference speed of Regenerative VFD (ACS800), like current speed is set as 0RPM, we wan to change to 50RPM.
How to change the reference speed of Regenerative VFD (ACS800), like current speed is set as 0RPM, we wan to change to 50RPM.
Answers
Hi
Your request is too general.
For example, why is the speed currently set to 0 RPM? What are the operating conditions of your motor?
However, the parameter where the speed is set also depends on the type of control you have ... are you using an analog reference? Are you using a fieldbus reference?
If you provide more information, maybe we can help you better
BR
Flavio
Your request is too general.
For example, why is the speed currently set to 0 RPM? What are the operating conditions of your motor?
However, the parameter where the speed is set also depends on the type of control you have ... are you using an analog reference? Are you using a fieldbus reference?
If you provide more information, maybe we can help you better
BR
Flavio
Add new comment