ABB Data Service Supervision not present in System 800xA 6.0.3
Hello,
I'm trying to Install and configure the IM in a virtual server using Windows server 2016 and System 800xA version 6.0.3.2, but after I've installed all the required applications, included the ABB Inform IT- Display Services I dont get the ABB Data Service Surpervision in the Windows services and doesn't Allow me to finish the configuration required by the Information Management Configuration Assistant.
Please your advice.
Best regards,
I'm trying to Install and configure the IM in a virtual server using Windows server 2016 and System 800xA version 6.0.3.2, but after I've installed all the required applications, included the ABB Inform IT- Display Services I dont get the ABB Data Service Surpervision in the Windows services and doesn't Allow me to finish the configuration required by the Information Management Configuration Assistant.
Please your advice.
Best regards,
Answers
It is unclear why you are not able to launch the ADSS interface. Note that you should be logged into the PC as the 800xA Service Account. I have attached a document describing how this can be accomplished via the MS Control Panel. I the MS Service for ADSS is not present, something has gone wrong with your installation. If this is the case, you should open a Support Case with your local Regional Support Center so that the tracking of the resolution of this issue can be documented.
Regards,
Geof Ledin
Regards,
Geof Ledin
Add new comment