COM MOD MAST
I can read the values of my first meter using com mod mast. while giving the other one I changed these things
SLAVE:2
changed the storage from mw0.0 to mw0.100
also added IEEE745_32B_to_REAL for converting the values to real because my meter readings are float
Is there anything else to change? I also changed the enables of two COM MOD MAST function blocks
SLAVE:2
changed the storage from mw0.0 to mw0.100
also added IEEE745_32B_to_REAL for converting the values to real because my meter readings are float
Is there anything else to change? I also changed the enables of two COM MOD MAST function blocks
Answers
This question has not yet been answered.
Add new comment