Ofsset in IEC 104 Addressing
Hi,
In the SYS600_IEC 60870-5-104 Master Protocol PDF, its mentioned that
"In SYS600 both the input and output process objects share the same address range, which means that there cannot be two process objects with overlapping addresses. If the same address is needed for an input and output object, it can be achieved by using offsets that are outside the information address range limited by the IL attribute."
How can I implement this offset, because in my case there is overlapping address between different process objects coming from the RTU 104 Server.
In the SYS600_IEC 60870-5-104 Master Protocol PDF, its mentioned that
"In SYS600 both the input and output process objects share the same address range, which means that there cannot be two process objects with overlapping addresses. If the same address is needed for an input and output object, it can be achieved by using offsets that are outside the information address range limited by the IL attribute."
How can I implement this offset, because in my case there is overlapping address between different process objects coming from the RTU 104 Server.
Thanks & Best Regards,
Jyothis M
✉ jyothis.m@kmrl.co.in | 🕿+919447787676
Answers
This question has not yet been answered.
Add new comment