pdf report not generating
in 800xA 6.0.1 we have ASCS 1 and ASCS2 earlier we in scheduler we defined reports which were generating in excel as well as PDF format but suddenly PDF format report are not generating.
please help
please help
Answers
ensure the scheduling node has access to Excell and the excel sheet you are using in the report. Also if you a 3rd party pdf creator it is also present
I am not sure if your question indicates that it was working in 6.0.1 and now it is not or if it was working in some other version and now it is not working in 6.0.1. I have two test systems. 800xA 6.0.3 & 800xA 6.1, and in both of these systems, the option is available.

If it was available in 6.0.1 and is not now, please look at your MS Event Viewer Log files for any indications of an error. Also, you should be able to look at the "ABBScheduler.log" file or the "ABBAction.log" file in the node where the Scheduler is running to possibly find some indications of any issues. Also ensure that the Acrobat Reader is available in the node where the Scheduler is running.
Regards,
Geof Ledin


If it was available in 6.0.1 and is not now, please look at your MS Event Viewer Log files for any indications of an error. Also, you should be able to look at the "ABBScheduler.log" file or the "ABBAction.log" file in the node where the Scheduler is running to possibly find some indications of any issues. Also ensure that the Acrobat Reader is available in the node where the Scheduler is running.
Regards,
Geof Ledin
Add new comment