S800 on Profinet


Hi,
has anyone successfully used AC800M with S800 on Profinet (CI871)?
When I am in the ABB Demo in the Cloud environment (800xA 6.1), I install the system extension Select IOs (according to online help)
I can add the CI871 in the ControlBuilder M, but when I try to add a device to the CI871, I cannot insert, because "insert unit" is greyed out. It looks like that CI845 is missing in S800 definitions for ProfiNet CI871
Any idea how to solve this?
br
Reinhard
Answers
The CI845 is in FCICI871HwLib Library, try adding this one to the Project, the same Library is used for CI845 for both Select I/O and S800.
I don't know why the "Insert Unit" is disabled in your case, does it mean you cannot add any other Profinet Devices as well?
Maybe try to create a new empty Control Builder Project and see if it works there.
I don't know why the "Insert Unit" is disabled in your case, does it mean you cannot add any other Profinet Devices as well?
Maybe try to create a new empty Control Builder Project and see if it works there.
Add new comment