ACS550: ID RUN (IDMAGNET) DOESN'T END
Hello,
I'm trying to do ID MAGN in order to work ACS550 in vector control mode. After defining motor data and pressing <I> key, ID RUN stars but after five minutes, it continues. Drive works in scalar control mode. Is there any way to restore drive (for example, 99.03 in ACS800)? Do you know why ID MAGN doesn't end?
I'm trying to do ID MAGN in order to work ACS550 in vector control mode. After defining motor data and pressing <I> key, ID RUN stars but after five minutes, it continues. Drive works in scalar control mode. Is there any way to restore drive (for example, 99.03 in ACS800)? Do you know why ID MAGN doesn't end?
Voted best answer
Hi
first, you should indicate the type of motor you would like to run in vector mode with the ACS550.
Better if you put a photograph of the motor plate.
Without this information, no hypothesis can be made.
To restore the scalar control mode, you must select it from parameter 99.04
BR
Flavio
first, you should indicate the type of motor you would like to run in vector mode with the ACS550.
Better if you put a photograph of the motor plate.
Without this information, no hypothesis can be made.
To restore the scalar control mode, you must select it from parameter 99.04
BR
Flavio
Add new comment