In ACS880 - 14 drive is not reaching the reference RPM?
Dear sir,
I am facing this problem in ACS880-14-***A-5 drives, in these drives I have given reference RPM = rated speed(1492,1485 etc.) and min speed limit is 1450rpm.
But the problem is that the drive is not reaching the reference rpm and running at min speed 1450rpm.
Pls see details given below -
I am facing this problem in ACS880-14-***A-5 drives, in these drives I have given reference RPM = rated speed(1492,1485 etc.) and min speed limit is 1450rpm.
But the problem is that the drive is not reaching the reference rpm and running at min speed 1450rpm.
Pls see details given below -
- Control Location - Ext 2
- Ref2 source - AI 2 scaled
- 22.01 reference unlimited - 1492
- Min speed - 1450rpm
- Max speed - 1492rpm
- AI 2 scaled ~=1492
Answers
This question has not yet been answered.
Add new comment