E: Internal complier error in file
HI
We build one logic in control builder M Professional. while checking within the diagram we are not getting any error.
but while doing download to soft controller, the download is not happening
Download was happening earlier.
There are 4 controller and one HI controller in the project. We are able to download in other nodes in soft controller, but particularly not able to download in node2. We are using 800xA 6.0.3-1, Control Builder M Professional is 6.0.0-1
error coming is as
"E:Internal compiler error in file fd\fdcollectmessagevisitor.cpp at line 415Error encountered while processing: POU-type N2_DCS_App1"
The screen shot is attached
We build one logic in control builder M Professional. while checking within the diagram we are not getting any error.
but while doing download to soft controller, the download is not happening
Download was happening earlier.
There are 4 controller and one HI controller in the project. We are able to download in other nodes in soft controller, but particularly not able to download in node2. We are using 800xA 6.0.3-1, Control Builder M Professional is 6.0.0-1
error coming is as
"E:Internal compiler error in file fd\fdcollectmessagevisitor.cpp at line 415Error encountered while processing: POU-type N2_DCS_App1"
The screen shot is attached
Answers
This question has not yet been answered.
by backdraft
The error means something like there is an error in your N2_DCS_App1 which prevents compiling the Code. I guess its a bug in Control Builder that you don't get it shown as Error on the Diagram itself already, but from the Message alone you cannot do much. Either attach an export of your Diagram here and hope for someone to look into it or open a case with ABB Supportline or both.
by Tomas Basista Rank: 621 on 3/11/2020 4:25:10 AM | Like (0) | Report
I had same error on 800xA v6.0.3. Deleted latest blocks from diagrams and error dissapeared.
Add new comment