PM858 licenses
Dear All,
when using Compact control builder with PM858 controller, what are the needed licenses for the CPU if i'm using the following,
3BSE066485R3 | F005 - PM851 Software License 800xA PM851K01/PM851AK01 Processor Unit License only.
Thank you in advance.
Abdelrazzaq Hiasat
when using Compact control builder with PM858 controller, what are the needed licenses for the CPU if i'm using the following,
- CI867K01 Modbus TCP Interface Package (for modbus communication with 3rd party systems)
- CI854BK01 PROFIBUS-DP/V1 (for ProfiBus communication with 3rd party systems)
- I have approximately 200 tags
3BSE066485R3 | F005 - PM851 Software License 800xA PM851K01/PM851AK01 Processor Unit License only.
Thank you in advance.
Abdelrazzaq Hiasat
Add new comment