dear sir I need gsd file for CI854A (in tia portal ) as master for connection with S1200 (CM1242-5)as slave. with
Answers
Hi,
AFAIK, CI854 A is a Profibus Master module, it does not have any GSD file to configure. To overcome this you need to use DP-DP coupler. which is used during Profibus communication for master to master module.
AFAIK, CI854 A is a Profibus Master module, it does not have any GSD file to configure. To overcome this you need to use DP-DP coupler. which is used during Profibus communication for master to master module.
Hi!
I guess that you are referring to the Simatic end of the communication?
Please observe that in the TIA portal sw, you need to configure the configuration as "DP slave" and the "Assigned DP Master" to "Not assigned", hence it is the ABB CI854 that is the DP master.
BR
Add new comment