how activate the anti-windup in a PID Gain Scheduling
I use the PID Gain schedule of the 800xA versao 6.0.3 system but the anti-windup is not working. Is there any way to activate this anti-windup. The PID output is not limited from the faceplate but shows that it assumes an output of 0-100. I don't know if the activation of this output is what activates the anti-windup. Somebody could help me. Thank you.
Answers
This question has not yet been answered.
by backdraft
What Type of PID Controller are you using (with Library Name and Version?)
The Output (ControlConnection Variable?) will usually have some kind of Min/Max Parameter to specify the Range which i guess in your case is 0..100 ?
Also it would help if you could provide your PID Parameters and example Trend of the case where it doesn't work...
Add new comment