Default folder S+ Engineering
Dear sirs,
We are using S+ Engineering 1.2 in our power plant. Since we have installed NAS (network attached storage) we would like to change project path on S+ Engineering. At the moment default path is C:\SymphonyPlus and we would like to change it to address one of the folders which we have created on NAS. How to do that?
We are using S+ Engineering 1.2 in our power plant. Since we have installed NAS (network attached storage) we would like to change project path on S+ Engineering. At the moment default path is C:\SymphonyPlus and we would like to change it to address one of the folders which we have created on NAS. How to do that?
Voted best answer
Believe that having S+Engineering projects on an NAS directory is not recommended at all, the project should always be on the local drive of the Composer server.
This to prevent database corruption in case of dropped packages and closed sockets.
If your goal is to have an backup you should instead setup some sort of automatic copy of the backup to the NAS drive in case of an drive failure on the server.
If your goal is to have several engineering stations you should use the server/client feature in S+Engineering or install a terminal server to host the project.
This to prevent database corruption in case of dropped packages and closed sockets.
If your goal is to have an backup you should instead setup some sort of automatic copy of the backup to the NAS drive in case of an drive failure on the server.
If your goal is to have several engineering stations you should use the server/client feature in S+Engineering or install a terminal server to host the project.
Add new comment