AC410 - Getting Error while translating the PC program into controller
Hi,
We are having one AC410 controller for Kiln Process, I am translating newly devoloped logics into existing PC program(PC30 - Recently created) into controller.
After some of FUNCM program translation i am getting 'INSUFFICIENT PC SPACE AVAILABLE' Error code. Kindly suggest weather it is required re-dimensioning of PC program or anything else can be done to overcome this error.
Present Dimensioning & Mstabs , PC programs & controller load detail screenshots attached. Kindly suggest in detail.
thanks in advance.
We are having one AC410 controller for Kiln Process, I am translating newly devoloped logics into existing PC program(PC30 - Recently created) into controller.
After some of FUNCM program translation i am getting 'INSUFFICIENT PC SPACE AVAILABLE' Error code. Kindly suggest weather it is required re-dimensioning of PC program or anything else can be done to overcome this error.
Present Dimensioning & Mstabs , PC programs & controller load detail screenshots attached. Kindly suggest in detail.
thanks in advance.
Answers
You need to backup the controller Database and Program tables with "DUDTB" and "DUTPT" commands, Initialize the controller, increase the PC Program Table Size with "DIMPC", and load the Database and Program Tables again with "LOTDB" and "LOTPT". The controller must be shut down for about an hour.
Note: Just because I told you what to do, doesn't mean you can just go ahead and assume everything is going to work without problems. I suggest you get on-site assistance from someone who has done this before.
Note: Just because I told you what to do, doesn't mean you can just go ahead and assume everything is going to work without problems. I suggest you get on-site assistance from someone who has done this before.
Hello.
Just to clarify a few more things.
As Rob says, take DUTDD & DUTPT dumps and cold start the controller, (clear init or reconfig).
Then load LOTDB and when you load the PC with LOTPT you get a question, do you want to redimension? and you answer yes and increase the
PC program table size.
As you can read when you type DIMPC you still have 1987 Kb free space in system so you can easily increase the PC size 500- 1000 Kb
You do not need to wait one hour like Rob says, I don't know where he got that from.
Just go on and reload and answer yes on redimension when loading LOTPT.
Best Regards Jan-Erik
Just to clarify a few more things.
As Rob says, take DUTDD & DUTPT dumps and cold start the controller, (clear init or reconfig).
Then load LOTDB and when you load the PC with LOTPT you get a question, do you want to redimension? and you answer yes and increase the
PC program table size.
As you can read when you type DIMPC you still have 1987 Kb free space in system so you can easily increase the PC size 500- 1000 Kb
You do not need to wait one hour like Rob says, I don't know where he got that from.
Just go on and reload and answer yes on redimension when loading LOTPT.
Best Regards Jan-Erik
Add new comment