Softcontroller xA 6.1
Hi!
I'm trying to use Softcontroller in xA 6.1 but can't find it in the menu.
AC 800M Softcontroller is deployed.
What else is there to do?
BR asp
I'm trying to use Softcontroller in xA 6.1 but can't find it in the menu.
AC 800M Softcontroller is deployed.
What else is there to do?
BR asp
Voted best answer
Is the Engineering Workplace feature assigned to the node where you lack Soft Controller?
Answers
Hi,
1. Check whether the softcontroller is deployed properly or not in SCC.
2. Try to find the softcontroller Panel from the following location C:\Program Files (x86)\ABB Industrial IT\Control IT\SoftController\SoftControllerPanel.exe
1. Check whether the softcontroller is deployed properly or not in SCC.
2. Try to find the softcontroller Panel from the following location C:\Program Files (x86)\ABB Industrial IT\Control IT\SoftController\SoftControllerPanel.exe
If its selected on the Node then the Node should either show Deploy needed or invalid. Otherwise you should contact support and send them your logs (Diagnostics option in System Setup).
Also you can try to install manually as workaround from
C:\ProgramData\ABB\800xA\MediaRepository\Engineering\AC800M_SoftController\ABB SoftController xA.msi
Also you can try to install manually as workaround from
C:\ProgramData\ABB\800xA\MediaRepository\Engineering\AC800M_SoftController\ABB SoftController xA.msi
The function AC 800M Softcontroller wasn't allocated to the nodes in System 800xA Configuration Console.
I allocated it and deployed. Now it works!
Thanks everyone for your input!
Br asp
I allocated it and deployed. Now it works!
Thanks everyone for your input!
Br asp
Add new comment