Mineral library automatic upload error
We are using 800xA and mineral library version 6.0.3
When we are using mineral library automatic upload program we faced some error and warning. And upload not happen. You can see these errors in attachment
How we can solve this problem?
When we are using mineral library automatic upload program we faced some error and warning. And upload not happen. You can see these errors in attachment
How we can solve this problem?
Answers
The relation between the 2 screenshots is not clear , is this from the same upload? If it's related, you may want to delete and re-create this object or run Consistency Check on this Application.
Else try to delete first everything under Minerals Library automatic upload object, then start the upload again.
Else try to delete first everything under Minerals Library automatic upload object, then start the upload again.
When choosing root in automatic upload just error happen but when choosing root/control network/project/application the error and warning happen
There is nothing under mineral library automatic upload for deleting.I cant delete mineral library automatic upload object in functional structure because this object is not in the object tree for recreate it.
And when we run consistency check it finishes without errors
Add new comment