FSD Util tool doesn`t read hwd file from project
Hi
I need to delete a bad configured hwd file from a control builder m 4.1.
I try to use the FSD Util tool .
In object name i write the path to the project: [Control Structure]Root/Control Network/DepuracionGases ; Aspect Name: Hardware Unit -> Error No aspect found!
In object name i write the path to the project: [Control Structure]Root.Control Network.DepuracionGases ; Aspect Name: Hardware Unit -> Error No aspect found!
Also tried
.
In object name i write the name of project: DepuracionGases ; Aspect Name: Hardware Unit -> Error No aspect found!
I looked for the path of the hwd files and copied to the object name with the same result.
I tried the same in the conectivity server and the aspect server.
When i open the project in the control builder i get the message : reading the hardware definitions file Projects\DepuracionGses\eh021551 and others hwd profibus files. I use this path and neither i can read the files with the FSD tool.
The question in how i have to access the hwd files in the FSD tool? How i have to write the path?
Where i have to do it. In the aspect server or the conectivity server where i have the control builder project?

Thanks in advance
José
I need to delete a bad configured hwd file from a control builder m 4.1.
I try to use the FSD Util tool .
In object name i write the path to the project: [Control Structure]Root/Control Network/DepuracionGases ; Aspect Name: Hardware Unit -> Error No aspect found!
In object name i write the path to the project: [Control Structure]Root.Control Network.DepuracionGases ; Aspect Name: Hardware Unit -> Error No aspect found!
Also tried
.
In object name i write the name of project: DepuracionGases ; Aspect Name: Hardware Unit -> Error No aspect found!
I looked for the path of the hwd files and copied to the object name with the same result.
I tried the same in the conectivity server and the aspect server.
When i open the project in the control builder i get the message : reading the hardware definitions file Projects\DepuracionGses\eh021551 and others hwd profibus files. I use this path and neither i can read the files with the FSD tool.
The question in how i have to access the hwd files in the FSD tool? How i have to write the path?
Where i have to do it. In the aspect server or the conectivity server where i have the control builder project?

Thanks in advance
José
Answers
This tool is not for beginners! Please file a support request at your regional ABB support center to get assistance.
Looks like you are using wrong aspect object path syntax.
Try using the same tool in a later system version to see how the path syntax is built up. Later versions have a browser to assist with getting the path extracted.
You can also copy the path off any object in Plant Explorer by right clicking its Structure Aspect and select Details...
I think the HWD files are stored on the CPU object. Use List Files to find it.
Looks like you are using wrong aspect object path syntax.
Try using the same tool in a later system version to see how the path syntax is built up. Later versions have a browser to assist with getting the path extracted.
You can also copy the path off any object in Plant Explorer by right clicking its Structure Aspect and select Details...
I think the HWD files are stored on the CPU object. Use List Files to find it.
Add new comment