Freelance HART DTM files connect
Hi ,
I want to ask about the procedures to connect hart DTM files to hardware structure in freelance engineering to achieve IAMS function.
I want to ask about the procedures to connect hart DTM files to hardware structure in freelance engineering to achieve IAMS function.
Answers
After inserting the PROFIBUS device (like S800 with CI801) as a FDT1.2 type slave and inserting a HART capable module like AO845 you select the module and click on "Insert..." in the context menu. A channel selection dialog pops up. You select the channel for your HART device and then select the DTM for this device from the opening list.
Add new comment