How to make Numeric Input Field
Sir, how can I make a numeric input field? because I can only find an alphanumeric display
Answers
The alphanumeric field covers both, text and numeric display. The format it uses depends on the type of the variable that is connected to it in the Process Value tab (for display)

and in the General tab - Action Button - Write Variable Selection - Write Variable field.

The display format can be configured in the Display tab - Format column by selecting one format from a selection (use F2 in the Format field) that is determined by the Variable connected in the Process Value Tab.

All the details can be found in the Engineering manual Operator Station Configuration, section "3 Graphics Display", sub-section "3.5 Animate, dynamic Graphic objects", chapter "3.5.19 Alphanumeric Display".
and in the General tab - Action Button - Write Variable Selection - Write Variable field.
The display format can be configured in the Display tab - Format column by selecting one format from a selection (use F2 in the Format field) that is determined by the Variable connected in the Process Value Tab.
All the details can be found in the Engineering manual Operator Station Configuration, section "3 Graphics Display", sub-section "3.5 Animate, dynamic Graphic objects", chapter "3.5.19 Alphanumeric Display".
Add new comment