Delete gsd or hwd files from a project in Control builder M 4.1
Hi
In my system I have a bad configured profibus instrument .
When I try to update the gsd file i get the message:
Hardware Definition Duplicated
File: C:\ABB Industrial IT Data\Enginner IT Data\ Control Builder M Professional 4.1\Projects\DepuracionGases\yp001555
The file contains duplicate hardware definitions or the hardware definition is already presente in the system. Check the log file sessionlog for further information
I want to delete the hwd file from the project but if i delete manually it appears again.
Could you help me?
Thanks in advance
José Pérez
In my system I have a bad configured profibus instrument .
When I try to update the gsd file i get the message:
Hardware Definition Duplicated
File: C:\ABB Industrial IT Data\Enginner IT Data\ Control Builder M Professional 4.1\Projects\DepuracionGases\yp001555
The file contains duplicate hardware definitions or the hardware definition is already presente in the system. Check the log file sessionlog for further information
I want to delete the hwd file from the project but if i delete manually it appears again.
Could you help me?
Thanks in advance
José Pérez
Answers
Hi Jose,
Was this problem solved?
Today I encountered the exactly same problem, could you advise how you solve it at the end?
Thank you.
Best regards,
Bill Lee
Was this problem solved?
Today I encountered the exactly same problem, could you advise how you solve it at the end?
Thank you.
Best regards,
Bill Lee
by Martin87 Rank: 104 on 12/23/2019 11:53:58 PM | Like (0) | Report
Have you tried removed it from the controlbuilder project?
by jperez Rank: 1751 on 12/25/2019 7:21:48 AM | Like (0) | Report
Yes.
I tried to update It with add mew hardware definition. Because i coud not.( I got a error message that said that the hardware was already un the project.) I tried to delete or rename the hwd file manually in the control buider project fólder.
But always the file appears again when i open again the control buider.
I tried to use the fsd útil tool. I was able yo list the hwd files if the project . When i deleted the wrong one. And list again the hwd files with the fsd it seemed deleted from the project but when i open again the control buider It appears again.
Then i tried to delete the file with fsd útil tool and then delete manually the file from the project fólder but the when i tried to open the project with control builder i got an error message asking for that file .
What i try to do is delete the hwd file so i doesnt apear in the list import ( when i add a new unit to the project) . Then i want to install the gsd well configured to be able yo use that type if instruments.
In the mean time i have install the hwd file of another instrument from a diferent manufacture but se want to unify replace parts so i still try to get the frist instrument wrigthly installed.
Thanks for tour kind help
Add new comment