800xA PMS Library Simulation on Soft controller
Hi
we upgraded PMS Library from 80xA version 5.0 PMS Library 5.0 to PMS 800xA Version 6.0.3 PMS library version 5.6 TC3. Upgrade is successful but now we stuck with simulation. when we forced value from hardware on soft controller we can see individual load value on face plate but PMS Main Sub LS didn't react on these values. or any other function of PMS. it seems we are missing something.
Is anybody share knowledge of simulation of PMS Library on soft controller.
we upgraded PMS Library from 80xA version 5.0 PMS Library 5.0 to PMS 800xA Version 6.0.3 PMS library version 5.6 TC3. Upgrade is successful but now we stuck with simulation. when we forced value from hardware on soft controller we can see individual load value on face plate but PMS Main Sub LS didn't react on these values. or any other function of PMS. it seems we are missing something.
Is anybody share knowledge of simulation of PMS Library on soft controller.
Answers
Few questions
1. SS CB A or B is closed?
2. LBB ID for SS Load is assigned?
3. Small or Large Lib is used? What is the Max Priority?
4. Is Net Size of your project is updated?
1. SS CB A or B is closed?
2. LBB ID for SS Load is assigned?
3. Small or Large Lib is used? What is the Max Priority?
4. Is Net Size of your project is updated?
Source:
Add new comment